Force converter

The Bossard Online Force Converter is used for converting different force units, such as newton, dyne, kilogram force, ounce force etc.


Please enter a valid number
 = 
Please enter a valid number

Instructions: First, select the respective force units to be converted. Next, enter a number into one of the two fields. The result is automatically converted after every change/entry.


Definition

The product of a mass and an acceleration equals force «F». Force is a fundamental variable for executing a work. Newton [N] is applied as physical unit in different applications and is partly named accordingly, such as the tensile force in tensile tests and the weight force during weighing.