Connected and intelligent tools and devices for process reliability and automation

Smart tools in assembly increase process reliability and productivity, resulting in significant savings potential leads.

They enable you to work independently of the control location. The tools can be connected to the system via WLAN, receive information about the next work step directly from the system and return information about the last work status such as torque, angle of rotation, time, current etc. Configuration of the tools is simple and user-friendly.

 

These are some advantages you will experience:

 

Qualität Schritt für Schritt  in der Produktion

Quality improvements

Continuous process monitoring during every fastening process and every interaction with the tool guarantees the correct processing for each fastening element in production.

Traceability

All process data are saved in a memory card. This ensures that the processing operations can always be are always traceable.

Leistungssteigerung in der Produktion

Highest flexibility

Up to 99 different operations can be stored directly in the mold and used in a single step, in a process process or in a sequence.

Improved productivity

The fitter can concentrate on the production production and not on the adjustments on the tool. This leads to to higher productivity.