according to ISO 898, part 2
1) If the description of the thread does not include thread pitch then the reference is to coarse threads (see ISO 261 and ISO 262).
Please start typing to get suggestions.
Vorschläge werden geladen.
according to ISO 898, part 2
1) If the description of the thread does not include thread pitch then the reference is to coarse threads (see ISO 261 and ISO 262).