New generation of direct fastened connections for plastics

Delta PT○

The successful Delta PT® screw has been further developed - the Delta PT® has an optimum geometry which favours the working of the plastic during the screwing process, and which reduces the damaging generation of heat.

There is a 50% higher tensional and torsional strength and a smaller thread pitch. Another development is the DELTA® CALC calculation program. Bossard's technical applications laboratory can employ this to determine the values and the details of the assembly parameters, working with original components provided by the customer.

DELTA PT® - The Screw for Thermoplastics