according to ISO 898, part 1

The revised standard as of April 2009 has been for the application for bolts, screws and studs with specified property classes – coarse thread and fine pitch thread.

Fasteners according to a product standard with reduced loadability need to be marked with property class preceded with the digit «0». The objective of the revised head marking is an indicative instruction for the assembly process. The user can further look up for additional notes in the Bossard catalogue. The revised head marking is a defined identification in accordance to the revised standard.

Judgement of the change for the user:
  • Fasteners that are manufactured according to the old standard have no functional differences compared to the revised standard.
  • Fasteners according to the mentioned specification are always subjected to reduced loadability due to the head geometry according to ISO 898-1 – this means that tightening torques has to be taken into account.

 

Download full chapter: Screws, bolts, nuts
Login to download the document (PDF) 

For the purpose of providing services, this website uses cookies. You will consent to this by clicking on “OK” and/or using our services.
Please click on privacy policy to find the information on cookies and the possibilities for modifying the terms of their storage.