It all began with guidance on fastening technology. For three years, we cultivated a relationship with Valley Enterprises, a company of Gemini Group, through consistent communication and exploratory projects. We successfully demonstrated the capabilities of our MultiMaterial-Welding® (MMW) technology in a load floor project for the Jeep Wrangler, which paved the way for a subsequent project with Stellantis’ Daytona/Charger. With the OEM already familiar with and confident in our solution, the project received swift approval.
The Challenges
Valley Enterprises had to transition from manually attaching brackets with screws and t-nuts to a machine-based ultrasonic welding process. This shift demanded trust in our new technology and required a substantial capital investment in ultrasonic welding machines. To address these concerns, our engineering team conducted multiple sample trials and prototypes, demonstrating superior performance over the existing method.
The performance of MMW technology met the OEM specifications and convinced Valley Enterprises of its efficacy. Moreover, the investment in the new machines was justified by comparable costs to current machines and labor expenses.
From 38 to 6 Pieces in Assembly Through a New Design

 Traditionally, connecting the bracket in the load floor required 3 t-nuts and 3 screws. With our innovative LiteWWeight® Pin, the pins and bracket are now fully integrated into a single piece. This integration reduces each bracket’s components from 7 or 5 to only 1 piece, eliminating 32 parts in total during the assembly process. This significant reduction not only shortens cycle time but also lowers material and labor costs.
Traditionally, connecting the bracket in the load floor required 3 t-nuts and 3 screws. With our innovative LiteWWeight® Pin, the pins and bracket are now fully integrated into a single piece. This integration reduces each bracket’s components from 7 or 5 to only 1 piece, eliminating 32 parts in total during the assembly process. This significant reduction not only shortens cycle time but also lowers material and labor costs.
Close Collaboration Key to Success
Introducing a new connection method posed both technical and economic challenges. Close collaboration and open communication with the OEM were crucial to ensure that the new technology met all required specifications and could be trusted to deliver as promised. Several sample trials and machine adjustments were necessary. However, this trial phase was completed smoothly and successfully. “The customer and the OEM were both very impressed and satisfied with the solution,” says Rob Tate, Business Development Manager at Bossard.
New Solution, Several Benefits
 The LiteWWeight® Pin geometry was licensed to Valley Enterprises for injection molding with the bracket together as one piece. We supported the client with machine design and sourcing to meet the requirements. The LiteWWeight® Pin functional integration delivers multiple key benefits:
The LiteWWeight® Pin geometry was licensed to Valley Enterprises for injection molding with the bracket together as one piece. We supported the client with machine design and sourcing to meet the requirements. The LiteWWeight® Pin functional integration delivers multiple key benefits:
- Eliminating 32 parts on the load floor
- More lightweight solution
- Faster cycle time
- Cost savings on components
The transition to ultrasonic welding and LiteWWeight® Pin technology streamlined their production process, resulting in a more efficient and cost-effective solution for the Stellantis Daytona/Charger load floors.
Talk to an expert for technology guidance