Buy Self-Tapping Screws for Plastic Online
Browse our assortment of direct assembly screws for plastic and order your fasteners online now.
Go to eShopFastening Technology
Find out what you need to consider when using self-tapping screws in plastic materials.

Self-tapping screws can form their own threads as they are driven into the parent material. With plastic, this requires a specially designed thread profile. Tapping screws used with steel, for example, could result in residual stresses in the plastic that might degrade the structural integrity of the assembly. You can avoid this with self-tapping screws specifically intended for plastic applications. They also give you more flexibility and allow quick assembly of components with fewer fasteners.
Browse our assortment of direct assembly screws for plastic and order your fasteners online now.
Go to eShopWhen looking into self-tapping screws, the first step is to decide what type is best suited for your specific application. In general, self-tapping screws for plastic are classified into two categories: thread-forming and thread-cutting.
To choose the right screw category, it’s important to understand the type of plastic you are fastening into: thermoplastic or thermoset.
Thread-forming screws generally function best in thermoplastic materials. They produce no waste because the plastic that is displaced to create the thread flows back into the root of the thread, resulting in a very secure fit.
For example, the ecosyn® plast is a great option for a thread-forming screw for plastic. These screws are designed to easily penetrate the material without causing stress. Other advantages of ecosyn® plast screws include:
Thread-cutting screws are designed for thermoset materials. These screws remove material because they have cutting edges. Thread-cutting screws have a smaller flank angle to reduce installation torque while increasing surface area, which results in a higher pullout force.
If you have further questions about self-tapping screws or need help in deciding on a fastener, please contact us. Our experts are happy to support you with guidance, technical advice, and assembly tests in our tech lab.


Digitalization
Supply chain disruptions are becoming increasingly common due to global pandemics, trade conflicts or natural disasters. This is how you keep up in such challenging times.

Read On
Read more interesting articles about supply chain management, fastening technology and more in our blog.