Expert Test Services

Tensile Strength and Compression Testing

Our test labs offer tensile and compression tests to assess the strength of metallic and composite materials. These tests determine yield strength, tensile strength, elongation at break, and other mechanical properties, ensuring precise quality assurance.

Engineer is conducting a tensile strength test in a technical test lab.
ATE | Tensile Testing Machine

YouTube Consent Required

This video is hosted by YouTube and requires Marketing Cookies to be accepted. Please accept Marketing Cookies to view the content.

Tensile testing machine to determine yield strength, tensile strength, elongation at break, and other mechanical properties

How Does a Tensile Strength Test Work?

Bossard has several testing facilities at its disposal to determine a material’s tensile strength. For example, tensile tests with a maximum of 600 kN can be performed for bolts and nuts from M3 to M33. During this process, your sample is stretched, shock-free, until it breaks or reaches a certain limit. The force (F) and the change in length are continuously measured on the sample and recorded during the test, allowing us to determine the load at which the sample begins to permanently deform – where the yield limit lies – and the load at which the material breaks – where the breaking load lies.

The Compressive Strength Test – The Reverse of the Tensile Test

Taking the direction of force into consideration, the compression test is the reverse of the tensile test. A compressive strength test provides information about a material’s behavior under uniaxial compression.

Tensile and Compression Tests in the Bossard Test Laboratory

As experts in fastening and materials technology, we perform all the tensile and compressive strength tests required for your quality assurance operations in our test laboratories.

Get Access to Bossard's Test Laboratory

As experts in fastening and materials technology, we perform all the tensile and compressive strength tests required for your quality assurance operations in our test laboratories.

Two men in a test lab examine a sewing machine on a desk in an industrial lab with additional workstations in the background. Key visual for Expert Test Services.

Contact Us for Tensile and Compression Testing

Please complete the form. *fields are required.