Force converter

The Bossard Online Force Converter is used for converting different force units, such as newton, dyne, kilogram force, ounce force etc.

 = 
 

Instructions: First, select the respective force units to be converted. Next, enter a number into one of the two fields. The result is automatically converted after every change/entry.

 

Definition

The product of a mass and an acceleration equals force «F». Force is a fundamental variable for executing a work. Newton [N] is applied as physical unit in different applications and is partly named accordingly, such as the tensile force in tensile tests and the weight force during weighing.


Verify your calculation, maximize potential of your product.

Bossard Expert Eduation
Could you or your engineering team use a refresher course on fastening technology? Visit Bossard Expert Education for available engineering seminars to consider!

Learn more

Bossard Expert Test Services
Want to verify your products are meeting quality standards? Test in one of our 14 certified testing laboratories worldwide (3 with a ISO/IEC 17025 certification).

Learn more