Beyond the Catalog: Why Aerospace Fastener Design Review Drives Weight, Safety, and Schedule
How weight reduction, surface treatment, and installation optimization protect performance across the aircraft lifecycle.
An aircraft can contain hundreds of thousands of fasteners. Each one is a small part, but each carries load, resists vibration, and has to keep doing so through thousands of flight cycles. In aerospace manufacturing, fasteners are engineered components that deserve the same design attention as the structures they hold together.
Too often, fastener selection happens late in the design process, as a catalog choice rather than an engineering decision. After more than 55 years in aerospace fastening, we've seen what happens when fasteners get a proper design review early: lighter assemblies, fewer surprises in qualification, smoother installation, and a more resilient supply chain.
Here is where that engineering effort pays off.
1. Weight Reduction: Every Gram Counts
In aerospace, weight is money and performance. Less mass means lower fuel burn, longer range, and greater payload capacity. Because a single airframe uses so many fasteners, even a small saving per part adds up across an assembly.
A rigorous design review looks at:
Material analysis: Is the current alloy the best fit for the load case, or could titanium or another high-strength, lower-density material do the job?
Structural optimization: Can the fastener geometry, head style, or length be refined to remove material that isn't contributing to strength?
Fastener count and layout: Can a joint be redesigned to achieve the same integrity with fewer or better-placed fasteners?
The goal is to shed unnecessary weight without compromising strength, fatigue life, or durability.
2. Physical Conditions: Designing for the Real Environment
Aerospace fasteners live in demanding conditions: wide temperature swings, vibration, pressure changes, moisture, fuel, hydraulic fluids, and de-icing chemicals. A fastener that performs well on the test bench can still fail early if the service environment was not fully considered.
Reviewing environmental suitability early lets engineers check that materials and designs hold up under thermal cycling, chemical exposure, and long-term mechanical stress. It also exposes risks such as galvanic corrosion when dissimilar materials meet, or stress corrosion in sensitive alloys. Catching these on paper is far cheaper than catching them in service.
3. Surface Treatments: Protection and Performance
Surface treatment is a functional part of the fastener design. The right coating or finish can:
Improve corrosion and wear resistance
Control friction for consistent installation torque and preload
Prevent galvanic reactions with surrounding materials
Extend service life and reduce maintenance intervals
Deliver a clean, consistent appearance
The right choice depends on base material, mating structure, operating environment, and applicable specifications. Optimizing the surface finish means matching all of these, so the fastener looks right and performs at its peak.
4. Obsolescence Management: Staying Ahead of the Supply Chain
Aircraft programs run for decades, but components and materials don't always last as long. A part that goes obsolete can interrupt a production line or complicate a fleet's maintenance plans.
Proactive obsolescence management means:
Identifying at-risk components before they become a problem
Evaluating qualified replacement options and equivalents
Planning transitions so production continues without disruption
Treating obsolescence as part of design review, not a crisis to react to, keeps programs on schedule.
5. Installation Process: Where Design Meets the Shop Floor
A well-designed fastener can still cause trouble if it's hard to install correctly. Installation errors lead to rework, delays, and quality escapes. Reviewing the installation process alongside the fastener itself helps teams:
Choose fasteners and procedures that reduce the chance of error
Specify appropriate tooling and techniques
Standardize practices across operators and sites
Shorten cycle times while maintaining quality
When the fastener, the tooling, and the process are designed as a system, installation becomes faster and more repeatable.
6. Production Optimization: The Bigger Picture
Looking beyond individual parts, a review of the manufacturing process can reveal inefficiencies that are easy to miss from inside the line: redundant steps, mismatched specifications, excess part variety, or quality checks that catch problems too late. Streamlining these, with strong quality control built in, improves throughput, consistency, and cost.
Why a 360° Approach Matters
These six areas are interconnected. A lighter fastener may need a different surface treatment. A new material may change the installation method. A coating decision may affect obsolescence risk. Optimizing one factor in isolation can create problems in another, which is why design review works best as a coordinated, whole-system effort.
That is the idea behind our 360° optimization: supporting customers with high-quality fasteners and with the engineering insight to get overall performance and efficiency from every fastening solution.
Let's Review Your Fastening Solutions
Whether you are launching a new program, refining an existing assembly, or facing an obsolescence challenge, an early design review can save weight, time, and cost. Contact us to discuss how a 360° optimization could improve your next project.